LPC55S6x High-speed PHY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S6x High-speed PHY

1,435件の閲覧回数
dingelen
Contributor III

Hi,

in the datasheet, for activating the high-speed PHY, it is mentioned the the 32k_osc should be activated. In the clock description section it is mentioned that this can be the FR32K or the XTAL32K.

Does it matter which of both is used for the High-speed PHY? I prefer not to add an extra external 32kHZ oscillator.

Thanks!

Tom

ラベル(2)
0 件の賞賛
返信
1 返信

1,348件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Tom,

 

You could use either external XTAL32K or internal FRO32K selecting from RTCOSC32KSEL register.

pastedImage_2.png

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信