LPC55S69JEV98

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69JEV98

815件の閲覧回数
tejas_Kt2i
Contributor I

Currently we are developing a product that requires sleep mode, and the controller itself is consuming 1.1mA but when we remove the power only for VDD pins, the functionality is still working, and the current consumption is dropped to 0.15 mA. 

This scenario we have seen in 2 boards out of 3 boards. where the 3rd board functionality itself failed when we removed the VDD connection

Attached the schematics snap

tejas_Kt2i_0-1748503791709.pngtejas_Kt2i_0-1748503791709.png

 

0 件の賞賛
返信
1 返信

753件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi @tejas_Kt2i 

 

  1. Do you mean that two  boards have issues when the VDD power is removed?
  2. Regarding "the third board failed when the VDD connection was removed": Please point out which specific functions failed.
  3. Note: VDD is the power supply for the I/Os.
  4. Please share the schematic in PDF format.

 

 

BR

Alice

 

0 件の賞賛
返信