LPC55S69 : wakeup due SPI3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 : wakeup due SPI3

1,834件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi !

SPI3 can be used as wakeup source for exit from PowerDown mode. And it works fine.

But RX fifo has size 8 items only and wakeup take > 350 us.

It means , MCU can't receive any more bytes until SPI ISR can be processed.

So I shouln't expect if more than 8 items will be in Fifo until exit from PowerDown is fully completed.

Is this so ? Or for wakeup more RX fifo can be allocated some how ?

Regards,

Eugene

ラベル(1)
1 返信

1,763件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Eugene,

You are right that the maximum FIFO size of LPC55S69 SPI module is 8, this is hardware restriction, no way to increase the SPI FIFO size.

If more than 8 data rush into the SPI FIFO before the exit from power-down is fully completed, some data will be lost.

Hope it can help you

BR

Xiangjun Rong