LPC55S69 : wakeup ADC for temperature measurement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 : wakeup ADC for temperature measurement

1,332件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi !

Temperature measurement in SDk example wakeup only 2 components in PMC:

/* Disable LDOGPADC power down */
POWER_DisablePD(kPDRUNCFG_PD_LDOGPADC);
/* Disable Temperature sensor power down. */
POWER_DisablePD(kPDRUNCFG_PD_TEMPSENS);

 Can it be so that we need one more line :

POWER_DisablePD(kPDRUNCFG_PD_GPADC);

Could you suggest right domains for temperature measurement only ?

I should measure temperature only few times per minute and would like to conserve energy as well.

What I should disable for be sure if all components what are involved in temperature measurements are not consume nothing. Or for better stability of temperature sensor I should keep it always ON ?

From other side I have PowerDown mode on sometines and during this mode, almost everything is powerd off automatically.

I assume, I can disable temp sensor all the time and enable it only for few ms when temperature result is really need.

Regards,

Eugene

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,246件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Eugene,

This is the components power down setting register.

But the temperature senor power down bit is reserved in the UM11126.pdf.

I think you should not power down the temperature sensor if you use it, because the temperature takes time to have the have temperature voltage stable.

BR

XiangJun Rong

pastedImage_1.png

0 件の賞賛
返信

1,246件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi xiangjun.rong‌ !

So I shouldn't powerdown temperature sensor, but I can powerdown ADC and LDO ADC.

Is this so ?

Regards.

Eugene

0 件の賞賛
返信

1,246件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Eugene,

Yes, You shouldn't powerdown temperature sensor, but you can powerdown ADC and LDO ADC.

BR

XiangJun Rong

0 件の賞賛
返信