LPC55S69 : temperature settling time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69 : temperature settling time

1,287 Views
EugeneHiihtaja
Senior Contributor I

Hello !

in DS is specified settling time of temperature sensor after power on in table 12.2.2

but what about settling time after Power-Down mode and actual conversion time ?

How fast after resuming from  Power-down mode I can get good measurement of temperature ?

Regards,

Eugene

0 Kudos
Reply
1 Reply

1,240 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Eugene,

As you may notice, this measure is not characterized but I think it would be a good aproximation to use the same setting time as the one from power-up. Also, this is an analog sensor connected to the channel 26 in the ADC so check the chapter 39.7.6 in the reference manual for more information about it.

Best Regards,

Alexis Andalon

0 Kudos
Reply