LPC55S69 : temperature measurement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 : temperature measurement

1,934件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi !

I'm follow lpcadc_temperature measurement and fins out that whole ADC initialization. calibration and skip first samples take at list 10 ms. ADC clock is 12 Mhz in my case.

I measure temperature after wakeup from PowerDown mode and I think this time is too much.

I can see all ADC settings are set in way to garantie as accurate measurement as possible.

But what is not clear if internal temperature sensor must be handled with those settings or we can set more relaxing values for ADC ?

I have tried to set :

g_LpadcCommandConfigStruct.sampleTimeMode = kLPADC_SampleTimeADCK19;
g_LpadcCommandConfigStruct.hardwareAverageMode = kLPADC_HardwareAverageCount32; // + calibration at 32

and can see that total procession time is reduced a lot.

Could you recommend as fast as possible setting for ADC what acceptable for handling temperature sensor in reliable way in whole temperature range.

Regards,

Eugene

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,843件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Eugene,

Regarding the two parameters:

g_LpadcCommandConfigStruct.sampleTimeMode = kLPADC_SampleTimeADCK19;
g_LpadcCommandConfigStruct.hardwareAverageMode = kLPADC_HardwareAverageCount32; // + calibration at 32

For the g_LpadcCommandConfigStruct.sampleTimeMode variable, it is dependent on the external signal source impedance, the smaller the signal source impedance is, the small value the g_LpadcCommandConfigStruct.sampleTimeMode variable should take.

For the g_LpadcCommandConfigStruct.hardwareAverageMode variable, the ADC converter samples multiple times and compute an average value.

As you know that the temperature sensor is a high impedance and stable signal, so you should assign big value for the g_LpadcCommandConfigStruct.sampleTimeMode variable, and assign small value for the g_LpadcCommandConfigStruct.hardwareAverageMode variable.

This is my opinion.

Hope it camn help you

BR

XiangJun Rong

0 件の賞賛
返信

1,843件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi xiangjun.rong‌ !

But can you suggest exact minimal values what garantie good result in whole temperature range and evaluated on NXP side ?

Regards,

Eugene

0 件の賞賛
返信

1,843件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Eugene,

Unfortunately, I can not give you the minimal value for the sample time parameter, because the temperature sensor impedance is not available.

BR

XiangJun rong

0 件の賞賛
返信