LPC55S69 : power down main oscillator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 : power down main oscillator

ソリューションへジャンプ
1,482件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hello !

I practice with Crystal-less clock configuration and haven't fins how -to powerdown main external oscillator.

For 32Khz one : POWER_EnablePD(kPDRUNCFG_PD_XTAL32K); /* Powered down the XTAL 32 kHz RTC oscillator */

But how-to power down main XTAL ?

Regards,

Eugene

ラベル(1)
0 件の賞賛
返信
1 解決策
1,408件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Eugene,

pls refer to the Table 292  in User Manual for LPC55S69.

In other words, you can set the PDEN_XTAL32K in Power configuration register 0 to power down the external 32K oscillator.

Hope it can help you

BR

Xiangjun Rong

pastedImage_2.png

元の投稿で解決策を見る

1 返信
1,409件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Eugene,

pls refer to the Table 292  in User Manual for LPC55S69.

In other words, you can set the PDEN_XTAL32K in Power configuration register 0 to power down the external 32K oscillator.

Hope it can help you

BR

Xiangjun Rong

pastedImage_2.png