LPC55S69: portSWITCH_TO_USER_MODE() is not defined

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69: portSWITCH_TO_USER_MODE() is not defined

1,643件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hello !

Do you have idea why macro portSWITCH_TO_USER_MODE()  is not defined for freertos  ?

Regards,

Eugene

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,587件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Eugene,

I have searched  "portSWITCH_TO_USER_MODE() " as a key words in google, the api function is related to MPU(memory protection unit), which can limit the resource scope a task can access. I think the freeRtos example does not use the function.

BR

XiangJun Rong

0 件の賞賛
返信

1,587件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi XiangJun Rong !

This macro must to be implemented as part of freertos port for LPC55.

But it missing.

Regards,

Eugene

0 件の賞賛
返信