LPC55S69 libpower_hardabi.a

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 libpower_hardabi.a

1,737件の閲覧回数
francisy
Contributor II

Hi, 

I use lpcxpresso55s69_power_manager_lpc with lpc55s69_evk. I am using SDK 2.7. 

sleep mode, deep sleep mode, deep power down mode work well.

But it cannot wake up from power down mode.

I change to use libpower_softabi.a and change the project config, architecture to FPV5-SP-D16(soft ABI), then it can wake up from power down mode. 

Is the libpower_hardabi.a buggy or do I need to do any extra configuration?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,654件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Francis,

Could you please confirm how you are attempting to wake up from power down.

I have attempted from my end but it works without any problems using the hardabi library.

I can wake up using the reset or the S1(ISP button).

I am using the SDK 2.7.0 and the LPCXpresso55S69 Rev A1

Best Regards,

Sabina

0 件の賞賛
返信