LPC55S69 : flash prefetch bit is dropped after PowerDown

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 : flash prefetch bit is dropped after PowerDown

1,446件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hello !

I'm setting Flash prefetch bit for accelerate performance.

Testing show that it set to 0 while PowerDown mode.

Is this true ?

Before :

+SYSCON->FMCCR 0xB03A  -> 150Mhz, prefetch ON

After:
-SYSCON->FMCCR 0x101A -> 12Mhz, prefetch OFF

Setting on FMCCCR in BOARD_BootClockFRO12M(); 

done in correct way.

Regards,

Eugene

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,404件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hi Eugene,

Could you please confirm the revision of your LPC55S69?

Can you please clarify what testing is done?

Testing show that it set to 0 while PowerDown mode.

Best Regards,

Sabina

0 件の賞賛
返信

1,404件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi sabinabruce‌ !

Everything is latest. Board revision A2.

When prefecth is enabled it is +25% gain in performance of software cryptography tests.

So prefecth is working if it enabled.

Regards,

Eugene

0 件の賞賛
返信