LPC55S69 : errata "ROM bootloader updated to provide API functionality for entry to ISP mode"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S69 : errata "ROM bootloader updated to provide API functionality for entry to ISP mode"

3,527 次查看
EugeneHiihtaja
Senior Contributor I

Hi !

I latest errata for LPC55S69 I can see :

"

5.1 ROM bootloader updated to provide API functionality for entry to ISP
mode
ISP.1: Devices with date code 2101 (yyww) and ROM patch version (T1.1.5), the ROM
bootloader will be updated to provide an API (runBootloader API) for the user application
to enter the ISP mode based on the designated ISP interface mode.

"

So basically this kind of ROM is only possible to have at beginning of the next year .

Regards,

Eugene

 

 

标签 (1)
0 项奖励
回复
4 回复数

3,518 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi Eugene,

Currently I am checking  this internally,

As soon I get feedback I will let you know.

BR,

Diego.

0 项奖励
回复

3,494 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @EugeneHiihtaja 


I just received confirmation from our applications team.

If you buy a part from Jan 2021 (and beyond) with the Rom patch versionT 1.1.5. 

 The run bootloader API (to invoke the bootloader from application code) will be available.

BR,

Diego.

3,479 次查看
EugeneHiihtaja
Senior Contributor I

Hi Diogo !

Do you have list of any other changes in Rom patch versionT 1.1.5. ?

 

Regards,

Eugene

 

0 项奖励
回复

3,440 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi Eugene,

Currently, I do not have further information regarding any other changes. However, if they are aimed to solve any issue, they probably will be mentioned in the errata sheet.

Regards,

Diego

0 项奖励
回复