LPC55S69 : errata "ROM bootloader updated to provide API functionality for entry to ISP mode"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 : errata "ROM bootloader updated to provide API functionality for entry to ISP mode"

3,607件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi !

I latest errata for LPC55S69 I can see :

"

5.1 ROM bootloader updated to provide API functionality for entry to ISP
mode
ISP.1: Devices with date code 2101 (yyww) and ROM patch version (T1.1.5), the ROM
bootloader will be updated to provide an API (runBootloader API) for the user application
to enter the ISP mode based on the designated ISP interface mode.

"

So basically this kind of ROM is only possible to have at beginning of the next year .

Regards,

Eugene

 

 

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,598件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi Eugene,

Currently I am checking  this internally,

As soon I get feedback I will let you know.

BR,

Diego.

0 件の賞賛
返信

3,574件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @EugeneHiihtaja 


I just received confirmation from our applications team.

If you buy a part from Jan 2021 (and beyond) with the Rom patch versionT 1.1.5. 

 The run bootloader API (to invoke the bootloader from application code) will be available.

BR,

Diego.

3,559件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi Diogo !

Do you have list of any other changes in Rom patch versionT 1.1.5. ?

 

Regards,

Eugene

 

0 件の賞賛
返信

3,520件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi Eugene,

Currently, I do not have further information regarding any other changes. However, if they are aimed to solve any issue, they probably will be mentioned in the errata sheet.

Regards,

Diego

0 件の賞賛
返信