LPC55S69: enable SRAM clocks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69: enable SRAM clocks

2,241 Views
EugeneHiihtaja
Senior Contributor I

Hi !

For worj with USB SRAM I should enable clock kCLOCK_UsbRam1 explictly in my code e.g. CLOCK_EnableClock(kCLOCK_UsbRam1). ConfigTool is also not generate this line in any mode.

But what about other SRAM /flash section and Flash ?

There are mentioned in clock_ip_t enumeration

kCLOCK_Sram1 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 3),
kCLOCK_Sram2 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 4),
kCLOCK_Sram3 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 5),
kCLOCK_Sram4 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 6),
kCLOCK_Flash = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 7),

Are the enabled by default ? Or BootROM enable those.

Or the managed by some PowerLib API or ROM api.

How to undestand ?

Regards,

Eugene

Labels (1)
0 Kudos
Reply
4 Replies

2,108 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi Eugene!

I am working on your question.

Please, provide me additional time to check

Regards,

Diego.

0 Kudos
Reply

2,108 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi Eugene!

Thank you for your patience,

On  the beginning of your application their controllers are already enabled by default, as we can see

on the following screenshot

pastedImage_3.png

Regards,

Diego

2,108 Views
EugeneHiihtaja
Senior Contributor I

Hi diego.charles‌ !

I can see in UM, default value for AHBCLKCTRL0 register is specified. It means SRAMn clocks enabled somewhere in bootrom. In this case is difficult to  trust if clocks always will be enabled there ( or disabled/enabled again ) and SRAM retain over reboot in next versions of bootrom if any.

By the way, I haven't found any clock enable for SRAM X area. Is this type of SRAM  always ON or it is just in other registers ?

But I think it is good idea to have clear spec. in what states registers remains after bootrom.

Regards,

Eugene

0 Kudos
Reply

2,108 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi Eugene,

You should not worry about the SRAM X areas, they are enabled by default.

As you know, you could control their retention state during low power modes using the sram_retention_ctrl register.

Regards,

Diego

0 Kudos
Reply