LPC55S69 : disable JTAG and SWD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 : disable JTAG and SWD

2,864件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hello !

Do I undestand right and SWD/JTAG ports are automatically disabled when Secure boot bit is activated ?

Regards,

Eugene

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,681件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Eugene Hiihtaja,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Do I understand right and SWD/JTAG ports are automatically disabled when Secure boot bit is activated?
-- No, I'm afraid not, and to provide the fastest possible support, I'd like to suggest you learn the detailed information about the secured JTAG via the link.
https://www.digi.com/resources/documentation/digidocs/90001546/concept/trustfence/c_secure_jtag.htm

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,681件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi !

But how it is applicable for LPC ?

If secure boot is not enabled, SWD debug works some how and may be enabled somewhere in ROM or where.

If I need to disable it I should follow UM Table 142. Debug Features Duplicate register (DEBUG_FEATURES_DP, offset = 0xFA8)

and disable debugging of CPU0, CPU1 and SWDs.

Or what exactly disabled if secure boot is enabled and what I should disable by myself for be secure ?

Thank you !

Regards !

Eugene

0 件の賞賛
返信

2,681件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Eugene Hiihtaja,

Thanks for your reply.
1) But how it is applicable for LPC?
-- Yes, and learn more information about it by reviewing 51.7 Debug authentication in the reference manual.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信