LPC55S69 dev board parodically requires hard reset to program it

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S69 dev board parodically requires hard reset to program it

3,897 次查看
plong44
Contributor II

I have an LPCXpresso55S69 dev board hooked up to a Jenkins server and periodically the board gets into a state where it is not flashable with the command line (using crt_emu_cm_redlink).

crt_emu_cm_redlink reports the following error:

PS Z:\> & $MCUX_IDE_BIN/crt_emu_cm_redlink --flash-mass-load-exec "file.bin" -p LPC55S69 --load-base=0x0 --bootromstall 0x50000040 --flash-driver= -x C:/<Project Path>/Debug --flash-dir $MCUX_FLASH_DIR0 --flash-dir $MCUX_FLASH_DIR1 --flash-hashing
Ns: MCUXpresso IDE RedlinkMulti Driver v11.3 (Jan 11 2021 16:41:13 - crt_emu_cm_redlink.exe build 9)
Wc(03). No cache support.
Nc: Found chip XML file in C:/<Project Path>/Debug\LPC55S69.xml
Nc: Restarted LinkServer process (PID 11896).
Ns: redlink server client - failed to receive response (to op 26) from server after 2000ms - timed out (rc 138)
Ns: redlink server client - failed to receive response (to op 26) from server after 2000ms - timed out (rc 138)
Ns: redlink server client - failed to receive response (to op 26) from server after 2000ms - timed out (rc 138)
Nc: Reconnected to existing LinkServer process.
Ns: redlink server client - failed to receive response (to op 26) from server after 2000ms - timed out (rc 138)
Nc: Server OK but no connection to probe 0 core -2(ANY) (after 3 attempts) - Ee(42). Could not connect to core.
Ed:02: Failed on connect: Ee(42). Could not connect to core.
Et:31: No connection to chip's debug port

 

Any hints or help resolving this issue would be much appreciated!

标签 (1)
0 项奖励
回复
7 回复数

3,888 次查看
converse
Senior Contributor V

Looks like the background process is having problems - make sure you kill the redlinkserv process before starting.

0 项奖励
回复

3,878 次查看
plong44
Contributor II

Thanks for the help Converse. I am not sure if it an issue with the background process on the computer, I do not see redlinkserv in the process list in between flashing attempts. I also just noticed that the issue persists across a reset of the computer, in my mind that points towards something go on with the dev board.

0 项奖励
回复

3,859 次查看
frank_m
Senior Contributor III

> I also just noticed that the issue persists across a reset of the computer, in my mind that points towards something go on with the dev board.

I don't think so.

I suspect an issue with the configuration and/or setup. I suppose the redlink server is a separate process, communicating via socket interface. Which means, it could be susceptible to firewall / virus scanner software.

3,851 次查看
plong44
Contributor II

That is an interesting point, I'll check the antivirus logs and whatnot for any evidence of interference. One thing that might not jive with your theory is that I am able to flash the board after I unplug it and plug it back in, if it was an antivirus/firewall issue I would think the problem would persist. Maybe that is a bad assumption though, thanks for help!

0 项奖励
回复

3,843 次查看
frank_m
Senior Contributor III

Usually such issues often turn up with remote debug, were debugger and debug server run on different machines.

To be honest, I am not much into MCUxpresso debugger details, but just assume it is similar to GDB. Most Eclipse toolchains run a separate GDB server process on the same machine, comunicating via Unix domain sockets (dunno how you call that on Windows...).

Perhaps you can locate the config/init script for the debug server, and modify it for more verbose output. That might give you a clue.

3,795 次查看
plong44
Contributor II

Thanks again for your help Frank. I ended up putting a relay (controlled by the PC) on the 5v line of a USB cable to allow me to programmatically reset the board. I'll probably try removing my relay board after the next mcuxpresso/windows/etc. update.

0 项奖励
回复

3,864 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

How about test on another PC?

0 项奖励
回复