LPC55S69 deep power down power estimation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69 deep power down power estimation

2,064 Views
gnichimohamed
Contributor III

Hello

For the LPC55S69, the current consumption in deep power down mode is 0.7uA with 4KB of SRAM retention. Does anyone know how much current the device consumes with 12KB of RAM retention instead?

Cheers.

0 Kudos
Reply
3 Replies

2,056 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to the Table 21 in data sheet of LPC55S69, different SRAM block consumes different current, for example, the 64K SRAM1 power supply current is about 11uA, so 12K SRAM1 consumes about 2uA.

Hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1621838037201.png

 

0 Kudos
Reply

2,052 Views
gnichimohamed
Contributor III

Thanks for the answer.

But that's in normal run mode, do you know how much it will consume in deep power down mode?

0 Kudos
Reply

2,045 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

We have not the current specs for the retaining RAM in low power mode, the RAM current spec in normal running mode can be a reference.

BR

XiangJun Rong

0 Kudos
Reply