LPC55S69 : adc reference voltages

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69 : adc reference voltages

2,430 Views
EugeneHiihtaja
Senior Contributor I

Hi !

In source code I can see the next enumeration :

/*!
* @brief Define enumeration of reference voltage source.
*
* For detail information, need to check the SoC's specification.
*/
typedef enum _lpadc_reference_voltage_mode
{
kLPADC_ReferenceVoltageAlt1 = 0U, /*!< Option 1 setting. */
kLPADC_ReferenceVoltageAlt2 = 1U, /*!< Option 2 setting. */
kLPADC_ReferenceVoltageAlt3 = 2U, /*!< Option 3 setting. */
} lpadc_reference_voltage_source_t;

But it is no any exact information in UM or DS about it.

Could you explain a bit  what option correspond to what settings ?

Regards,

Eugene

Labels (1)
3 Replies

2,321 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Eugene Hiihtaja,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
The enum value is used to select the voltage reference as below shows.

pastedImage_1.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,321 Views
EugeneHiihtaja
Senior Contributor I

Hi jeremyzhou‌ !

Could you confirm if VREFP is implemented on scheme of LPC55S69-EVK in correct way.

I can see it connected to VDDA_TARGET. Or in this way it is good enough  reference voltage for ADC ?

br,Eugene

0 Kudos
Reply

2,321 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Eugene Hiihtaja,

1) In this way it is good enough  reference voltage for ADC ?

-- Yes, it's Ok.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------