LPC55S69 USB1 HS PHY PLL initialization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69 USB1 HS PHY PLL initialization

1,274 Views
pettel
Contributor II

The documentation (UM11126, Rev. 2.8, Table 850) says for Bit 21 PLL_REG_ENABLE:

SW must set this bit 15 us before settiing PLL_POWER to avoid glitches on PLL output clock.

 

When I look in the source code of the the SDK (Version 25.6.0) into fsl_clock.c:
2045 │ /* Enable USB PHY clock */
2046 │ bool CLOCK_EnableUsbhs0PhyPllClock(clock_usb_phy_src_t src, uint32_t freq)
....

2120 │ USBPHY->PLL_SIC = (USBPHY->PLL_SIC & ~USBPHY_PLL_SIC_PLL_DIV_SEL(0x7)) | phyPllDiv;
2121 │ USBPHY->PLL_SIC_SET = USBPHY_PLL_SIC_SET_PLL_REG_ENABLE_MASK;
2122 │ USBPHY->PLL_SIC_CLR = (1UL << 16U); // Reserved. User must set this bit to 0x0
2123 │ USBPHY->PLL_SIC_SET = USBPHY_PLL_SIC_SET_PLL_POWER_MASK;
2124 │ USBPHY->PLL_SIC_SET = USBPHY_PLL_SIC_SET_PLL_EN_USB_CLKS_MASK;
2125 │
2126 │ USBPHY->CTRL_CLR = USBPHY_CTRL_CLR_CLKGATE_MASK;

 

PLL_REG_ENABLE is set in line 2121 and PLL_POWER is set in line 2123 with no regard for the 15 us time delay required in the user manual. Is this function in fsl_clock.c flawed or am I missing something?

0 Kudos
Reply
1 Reply

1,229 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @pettel 

I have reviewed both the UM11126 and the SDK  implementation for enabling the USB PHY PLL.
According to the UM, software must set the PLL_REG_ENABLE bit at least 15 microseconds before setting PLL_POWER to avoid glitches on the PLL output clock:

ZhangJennie_0-1758513929134.png

However, in the current SDK implementation (fsl_clock.c), PLL_REG_ENABLE and PLL_POWER are set consecutively without any delay in between.

To ensure reliable operation, I suggest adding a 15-microsecond delay between setting PLL_REG_ENABLE and PLL_POWER.

I will report it to the SDK team meanwhile. Thank you so much for bringing the problem to our attention.

Best Regards

Jun Zhang

0 Kudos
Reply