LPC55S69 : SRAMX_3 usage for CPU retention data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69 : SRAMX_3 usage for CPU retention data

5,119 Views
EugeneHiihtaja
Senior Contributor I

Hi !

Hi !

 

In UM mentioned that is possible to select SRAMX area for CPU retention :

 

"If CPU retention used in power-down mode, SRAMX_2 (0x1400 6000 to 0x1400 65FF) is
used (total 1.5 KB) by default in power API and this is user configurable within SRAMX_2 and SRAMX_3.

"

 

But it is not clear how-to configure in use SRAMX_3 area instead of SRAMX_2 for save CPU retention data.

 SRAM_X3 should be retained if it used and it can be configured bit how-to redirect CPU data is not clear.

 

Regards,

Eugene

Labels (1)
0 Kudos
Reply
9 Replies

5,048 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Eugene Hiihtaja 

We use ROM API POWER_EnterDeepPowerDown to configure in use SRAMX  area.

The sram_retention_ctrl parameter defines which SRAM instances will be put in Retention mode during deep power-down. SRAM instances in Retention mode do not lose their content. SRAM instances that are not required to be put in Retention mode during deep power-down will be shut down (meaning their content will be lost upon wake-up from deep
power-down.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

5,048 Views
EugeneHiihtaja
Senior Contributor I

Hi ZhangJennie‌ !

I'm using POWER_EnterPowerDown() API and it is quite clear what exact SRAM areas should be retain by specifying mask sram_retention_ctrl . 0x7FFF is cover whole SRAM space.

BUT

 

in UM:

"If CPU retention used in power-down mode, SRAMX_2 (0x1400 6000 to 0x1400 65FF) is
used (total 1.5 KB) by default in power API and this is user configurable within SRAMX_2 and SRAMX_3.

"

"

If CPU retention used in power-down
mode, SRAMX_2 (0x1400 6000 to 0x1400 65FF) is
used (total 1.5 KB) by default in power API and this is
user configurable within SRAMX_2 and SRAMX_3.

"

SRAMX  ( 0x1400 0000 - 0x1400 7FFF, size 32KB )


             SRAMX_0  -  0x1400 0000 -  0x1400 1FFF
             SRAMX_1  -  0x1400 2000 -  0x1400 3FFF
             SRAMX_2  -  0x1400 4000  - 0x1400  5FFF
             SRAMX_3  -  0x1400 6000  - 0x1400  7FFF,              --> 0x1400 6000 to 0x1400 65FF  ( CPU retention area )

So really it is ín SRAMX_3 already but can be in X_2 as well ?

Or how I should understand CPU retention area location ?

Regards,

Eugene

0 Kudos
Reply

5,048 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Eugene,

The size of RAM_X0 to RAM_X3 is not same, see table 307 in UM

pastedImage_1.png

So 0x1400 6000 to 0x1400 65FF  ( CPU retention area ) is inside RAM_X2 instance.

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

5,048 Views
EugeneHiihtaja
Senior Contributor I

Hi ZhangJennie‌ !

I need large contiguous area of SRAMX and would like to move CPU retention area to  SRAM_X3

, like it mentioned in UM.

"If CPU retention used in power-down mode, SRAMX_2 (0x1400 6000 to 0x1400 65FF) is
used (total 1.5 KB) by default in power API and this is user configurable within SRAMX_2 and SRAMX_3.

"

How it can be done ?

Regards,

Eugene

0 Kudos
Reply

5,048 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

config sram_retention_ctrl is used to set retained RAM.

for example, with below code, RAM instances RAM_X2 & RAM_X3 content will be retained.

sram_retention_ctrl = LOWPOWER_SRAMRETCTRL_RETEN_RAMX2 |
LOWPOWER_SRAMRETCTRL_RETEN_RAMX3; 

this chip doesn't have feature to set large contiguous area of SRAMX for CPU retention area.

0 Kudos
Reply

5,048 Views
EugeneHiihtaja
Senior Contributor I

Hi ZhangJennie‌ !

So this memory area : SRAMX_2 (0x1400 6000 to 0x1400 65FF)  is hardcoded for CPU retention data in case of PowerDown mode

and can't be changed. Is this so ?

Regards,

Eugene

0 Kudos
Reply

5,048 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

yes, correct.

0 Kudos
Reply

5,048 Views
EugeneHiihtaja
Senior Contributor I

Hi ZhangJennie‌ !

But for what reason SRAMX_3 area is mentioned there ?

It should be reason or this is typo or nondocumented feature ?

Moving CPU retention data from SRAMX2 to 3 will bring extra 4KB of SRAM and it good benefit.

Regrads,

Eugene

0 Kudos
Reply

5,048 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

UM is right. not typo

0 Kudos
Reply