LPC55S69 I2S Record (Rx) examples

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 I2S Record (Rx) examples

ソリューションへジャンプ
2,389件の閲覧回数
sanders7284
Contributor III

Trying to interface to a CMX655D codec via I2S.

I have all the right signals int the right places and have checked all the IRQ are enabled in the NVIC and Flexcomm. Despite this I have no IRQ being generated.

Just wondering if there are any examples of I2S Record (Rx) all the SDK examples are play (Tx).  

Regards

0 件の賞賛
返信
1 解決策
2,371件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 

Please refer MCUXpresso I2S SDK demo code

SDK_2.8.2_LPCXpresso55S69\boards\lpcxpresso55s69\driver_examples\i2s

 

Hope this helps,

Jun Zhang

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,371件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 

Please refer MCUXpresso I2S SDK demo code

SDK_2.8.2_LPCXpresso55S69\boards\lpcxpresso55s69\driver_examples\i2s

 

Hope this helps,

Jun Zhang

0 件の賞賛
返信
2,358件の閲覧回数
sanders7284
Contributor III

Thanks Jun Zhang,

I was looking at the wrong SDK, which is why I could only see Tx.

Regards

0 件の賞賛
返信