LPC55S69 : Gpio pin configurations

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S69 : Gpio pin configurations

1,307 次查看
EugeneHiihtaja
Senior Contributor I

Hello !

In UM is mentioned that  Pull-up/pull-down resistor can be configured for almost any GPIO pin.

But it is not clear if resistors available when pin configured as input or output.

Or it dosn't matter , both resistors available for input and output pins like ?

Regards,

Eugene

0 项奖励
回复
1 回复

1,193 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Eugene Hiihtaja,

Yes,  it dosn't matter , both resistors available for input and output pins .


Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------