LPC55S69 : FMC configuration register

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 : FMC configuration register

1,620件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hello !

I can see in all examples in SDK is only FLASHTIM is set .

But what about enable flash prefetch and acceleration bits ?

They never enabled. Why ? They should work with silicon 1B.

How to handle those ?

Can I enable those at the same time when FLASHTIM is changed ?

Should I invalidate/flush those caches when use Flash API from Bootrom ?

Or when I encrypt/decrypt on fly if PRINCE peripheral is in use.

In K82 time it was always separate API to handle those issues.

Regards,

Eugene

0 件の賞賛
返信
2 返答(返信)

1,530件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Eugene, 

But what about enable flash prefetch and acceleration bits ?

They never enabled. Why ? They should work with silicon 1B.

Yes you should be able to enable these without a problem. The SDK examples are not designed to show the optimum behavior, instead we provide base examples that show how the peripherals should work. Though any additional modifications to optimize or customize should be made by customers.

How to handle those ?

Can I enable those at the same time when FLASHTIM is changed ?

You may enable them as you mention. However please consider the following points.

pastedImage_5.png

Please confirm the revision you are working with and disable the prefetch bit must be disabled prior to executing flash commands.

Best Regards,

Sabina

0 件の賞賛
返信

1,530件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi Sabina !

Yes, I have A2 board revision and expect there 1B version of bootloader.

Regards,

Eugene

0 件の賞賛
返信