LPC55S69 FLEXCOMM3 RX not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC55S69 FLEXCOMM3 RX not working

跳至解决方案
2,071 次查看
nxf51434
NXP Employee
NXP Employee

As the title, customer test the uart3(flexcomm3) on EVK and found the uart3 can send data successfully but can't receive data. They test other uarts like uart1 and uart7, all can work properly. @Logiase.song

 

0 项奖励
回复
1 解答
2,065 次查看
Logiase
NXP Employee
NXP Employee

Logiase_0-1701671885803.png

connect P1 solve this problem.

The level translator change the pull level of P0_3 (rx). 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,065 次查看
Logiase
NXP Employee
NXP Employee

Logiase_0-1701671885803.png

connect P1 solve this problem.

The level translator change the pull level of P0_3 (rx). 

0 项奖励
回复
2,057 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I see your phenomenon, close P1, the BRIDGE_OE pin will be high, U6 and U3 will be disabled, the pins of U3 and U6 will be float, if you connect the external uart transmit signal to FC3_RXD pin(PIO0_3), in detail  pin 3 of P20, it will function.

BR

XiangJun Rong

0 项奖励
回复