LPC55S69-EVK revision A3 files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69-EVK revision A3 files

Jump to solution
1,654 Views
aashish1
Contributor I

Dear ALL,

Greetings!!

I just bought LPC55S69-EVK for my learning, but the board revision is A3 (700-35089 rev A3, SCH-35089 rev A3, EA-W01023-2489 mentioned on the board).

The design files that are available on the NXP's product page for LPC55S69-EVK has the schematic and design files only for rev A1/A2.

Please tell me if the rev A3 has no design related changes from rev A2 ? 

If rev A3 has design related changes from rev A2 what are those changes ?

Or, can somebody share me the schematic and design files for the rev A3 of LPC55S69-EVK board, as I need them for my study and board usage.

Thanks.

0 Kudos
Reply
1 Solution
1,632 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @aashish1 

You can totally refer to the Schematic for A1/A2. There is no difference for the customer. My board is also A3, and I have been using SCH A1 all the time.

 

BR

Alice

View solution in original post

0 Kudos
Reply
2 Replies
1,608 Views
aashish1
Contributor I

Great thanks for your support sir.

0 Kudos
Reply
1,633 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @aashish1 

You can totally refer to the Schematic for A1/A2. There is no difference for the customer. My board is also A3, and I have been using SCH A1 all the time.

 

BR

Alice

0 Kudos
Reply