LPC55S69 EVK - Wire ACK Error during Debug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC55S69 EVK - Wire ACK Error during Debug

跳至解决方案
12,345 次查看
SrinathVelavan
Contributor III

Hi, 

I am getting the following errors while debugging using LPC55S69 EVK. I am running the B2B SPI example from the SDK for testing. Build process clears without any error but I get this error during Debug. 

Any solutions? Also is there a way to factory reset the LPC55S69 EVK board like reflashing to factory new settings?

 

NOTE: Attached screenshots for reference

#LPC55S69

标签 (1)
0 项奖励
回复
1 解答
12,308 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Thanks for the sharing. Good to know the problem got solved.

If the problem can be resolved by entering ISP mode, the reason should be your onchip application disturbing debug connection. eg, program in low power mode, watchdog reset, etc.

Entering ISP can bypass the running application.

Jun Zhang 

在原帖中查看解决方案

5 回复数
12,337 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @SrinathVelavan 

Could you please try to download led_blinky demo code. Is the problem the same?

Thanks,

Jun Zhang

0 项奖励
回复
12,317 次查看
SrinathVelavan
Contributor III

Hi, 

We solved the issue. Just needed to change the Jumper settings on the EVK to ISP mode and the led blinky code compiled and debugged. 

 

Thanks for your help

0 项奖励
回复
12,309 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Thanks for the sharing. Good to know the problem got solved.

If the problem can be resolved by entering ISP mode, the reason should be your onchip application disturbing debug connection. eg, program in low power mode, watchdog reset, etc.

Entering ISP can bypass the running application.

Jun Zhang 

12,297 次查看
SrinathVelavan
Contributor III
Thanks for this valuable info.
0 项奖励
回复
12,322 次查看
SrinathVelavan
Contributor III

Facing the same issue.

0 项奖励
回复