LPC55S69 EVK - Wire ACK Error during Debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 EVK - Wire ACK Error during Debug

ソリューションへジャンプ
12,035件の閲覧回数
SrinathVelavan
Contributor III

Hi, 

I am getting the following errors while debugging using LPC55S69 EVK. I am running the B2B SPI example from the SDK for testing. Build process clears without any error but I get this error during Debug. 

Any solutions? Also is there a way to factory reset the LPC55S69 EVK board like reflashing to factory new settings?

 

NOTE: Attached screenshots for reference

#LPC55S69

ラベル(1)
0 件の賞賛
返信
1 解決策
11,998件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Thanks for the sharing. Good to know the problem got solved.

If the problem can be resolved by entering ISP mode, the reason should be your onchip application disturbing debug connection. eg, program in low power mode, watchdog reset, etc.

Entering ISP can bypass the running application.

Jun Zhang 

元の投稿で解決策を見る

5 返答(返信)
12,027件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @SrinathVelavan 

Could you please try to download led_blinky demo code. Is the problem the same?

Thanks,

Jun Zhang

0 件の賞賛
返信
12,007件の閲覧回数
SrinathVelavan
Contributor III

Hi, 

We solved the issue. Just needed to change the Jumper settings on the EVK to ISP mode and the led blinky code compiled and debugged. 

 

Thanks for your help

0 件の賞賛
返信
11,999件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Thanks for the sharing. Good to know the problem got solved.

If the problem can be resolved by entering ISP mode, the reason should be your onchip application disturbing debug connection. eg, program in low power mode, watchdog reset, etc.

Entering ISP can bypass the running application.

Jun Zhang 

11,987件の閲覧回数
SrinathVelavan
Contributor III
Thanks for this valuable info.
0 件の賞賛
返信
12,012件の閲覧回数
SrinathVelavan
Contributor III

Facing the same issue.

0 件の賞賛
返信