LPC55S69 EVK - Wire ACK Error during Debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69 EVK - Wire ACK Error during Debug

Jump to solution
12,303 Views
SrinathVelavan
Contributor III

Hi, 

I am getting the following errors while debugging using LPC55S69 EVK. I am running the B2B SPI example from the SDK for testing. Build process clears without any error but I get this error during Debug. 

Any solutions? Also is there a way to factory reset the LPC55S69 EVK board like reflashing to factory new settings?

 

NOTE: Attached screenshots for reference

#LPC55S69

Labels (1)
0 Kudos
Reply
1 Solution
12,266 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Thanks for the sharing. Good to know the problem got solved.

If the problem can be resolved by entering ISP mode, the reason should be your onchip application disturbing debug connection. eg, program in low power mode, watchdog reset, etc.

Entering ISP can bypass the running application.

Jun Zhang 

View solution in original post

5 Replies
12,295 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @SrinathVelavan 

Could you please try to download led_blinky demo code. Is the problem the same?

Thanks,

Jun Zhang

0 Kudos
Reply
12,275 Views
SrinathVelavan
Contributor III

Hi, 

We solved the issue. Just needed to change the Jumper settings on the EVK to ISP mode and the led blinky code compiled and debugged. 

 

Thanks for your help

0 Kudos
Reply
12,267 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Thanks for the sharing. Good to know the problem got solved.

If the problem can be resolved by entering ISP mode, the reason should be your onchip application disturbing debug connection. eg, program in low power mode, watchdog reset, etc.

Entering ISP can bypass the running application.

Jun Zhang 

12,255 Views
SrinathVelavan
Contributor III
Thanks for this valuable info.
0 Kudos
Reply
12,280 Views
SrinathVelavan
Contributor III

Facing the same issue.

0 Kudos
Reply