LPC55S69 Debug Problem with JLink V9

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S69 Debug Problem with JLink V9

2,297 次查看
wmp
Contributor I

Recently i have made an LPC55S69 basic-system PCB  equiped with a standard SWD(SWCLK,SWDIO,SWO and RESET signal) Debug probe.But when i conneted my jlink to the board and pressed debug button in mcuxpresso ide with an opened example GPIO project import from the SDK,errors showed "connot connect to the tartget".However,the debugger has detected the mcu's Model.

I have checked my PCB routes and SCH connections,it seems I have made everthing properly, 10K pull-up resistor on SWCLK and SWDIO or default jtag pin connections.

Did anybody ever make a circuit board based on this mcu?Could anyone tell me the debug result about his own board?20191224215406.png

标签 (1)
0 项奖励
回复
1 回复

2,042 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi WM

Please refer this article to design your debug interface

Design Considerations for Debug 

Have a nice day

Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复