LPC55S69 Ctimer CAP question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S69 Ctimer CAP question

1,276 次查看
qingyunliu
Contributor II

1. Does Ctime CAP must triggered by external PIN? Could we use internal configure to measure some PINs frequency.

2. Does LPC55S69 Ctimer CAP abality has limit? eg. I want use Ctimer CAP to measure 48KHZ clock.

标签 (1)
0 项奖励
回复
1 回复

1,249 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @qingyunliu 

1. I did not understand if you are refering: how the capture is triggerd to get the value or how the input signal is provided to the mcu.

2. The CAP frequency limit is defined with the APB bus clock. On chapter 25.6.11 Count Control Register of the user manual says "the frequency of the CAP input cannot exceed one half of the
APB bus clock" also on chapter 4.4.1 Clock generation says "The maximum allowed frequency for main clock and system clock (to CPU0, CPU1, AHB bus, Sync, etc.) is 150 MHz".

I'll be waiting for the clarification to question 1.

Best Regards, Miguel.

0 项奖励
回复