LPC55S69 : 1-bit SPI NOR FLASH support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S69 : 1-bit SPI NOR FLASH support

1,793 次查看
EugeneHiihtaja
Senior Contributor I

Hello !

In UM mentioned about NOR flash memory support in ROM code directly :

8.6.11.2 1-bit SPI NOR FLASH support (for version 1B only)   and it can be programmed by using blhost.

But it is not clear to what SPI interface it can be connected and how to initialize it  ( if need ).

What about ROM api what use used for work with SB file ?

Can they work directly with this NOR memory ?

Regards,

Eugene

标签 (1)
0 项奖励
回复
2 回复数

1,675 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Eugene,

I have to admit that the part in UM11126.pdf is confused and unclear, I have asked AE team, I will give you a reply after I get a feedback.

BR

XiangJun Rong

0 项奖励
回复

1,675 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Eugene,

I get feedback from AE team, the FlexComm3 module is used as single I/O SPI NOR flash interface as the following fig.

Hope it can help you

BR

Xiangjun Rong

https___community.nxp.com_servlet_JiveServlet_showImage_2-1244799-293593_pastedImage_1.png

0 项奖励
回复