LPC55S69 : 1-bit SPI NOR FLASH support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69 : 1-bit SPI NOR FLASH support

1,813 Views
EugeneHiihtaja
Senior Contributor I

Hello !

In UM mentioned about NOR flash memory support in ROM code directly :

8.6.11.2 1-bit SPI NOR FLASH support (for version 1B only)   and it can be programmed by using blhost.

But it is not clear to what SPI interface it can be connected and how to initialize it  ( if need ).

What about ROM api what use used for work with SB file ?

Can they work directly with this NOR memory ?

Regards,

Eugene

Labels (1)
0 Kudos
Reply
2 Replies

1,695 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Eugene,

I have to admit that the part in UM11126.pdf is confused and unclear, I have asked AE team, I will give you a reply after I get a feedback.

BR

XiangJun Rong

0 Kudos
Reply

1,695 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Eugene,

I get feedback from AE team, the FlexComm3 module is used as single I/O SPI NOR flash interface as the following fig.

Hope it can help you

BR

Xiangjun Rong

https___community.nxp.com_servlet_JiveServlet_showImage_2-1244799-293593_pastedImage_1.png

0 Kudos
Reply