LPC55S36-EVK no contact via debugger after running TrustZone example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S36-EVK no contact via debugger after running TrustZone example

814 Views
jpholme
Contributor II

I have tried out the TrustZone examples that comes with the LPC55S36 SDK from NXP's website using the IAR EWARM environment. I could debug this nicely and jump from secure start-up into the nonsecure part of the simple Hello World example.

Suddenly, however, I am locked out and can't debug anymore. Using BLHOST and starting the ISP-bootloader, I can run a ".... get-property 17" and see that the bootloader is now in SECURE mode. How did it jump in there? 

And I suppose this is irreversible?

And can I do anything to get back to debyugging?

0 Kudos
Reply
1 Reply

794 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, could you let me know what was the example that you using? I will replay on my side.

Best regards,
Pavel

0 Kudos
Reply