LPC55S28 using UAC2.0 change audio sample rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S28 using UAC2.0 change audio sample rate

Jump to solution
1,477 Views
PatrickLai
Contributor III

Hi,

I am testing UAC2.0 with sample code dev_composite_hid_audio_unified_freertos, SDK version is 24.12.00/25.09.00. After directly import the sample code from the SDK, I made the following change, but both the recorder and the speaker cannot work. Please provide some suggestions or solutions. Thanks!

PatrickLai_0-1759288666683.png

 

0 Kudos
Reply
1 Solution
1,423 Views
PatrickLai
Contributor III
need to reinstall the driver for the device

View solution in original post

0 Kudos
Reply
1 Reply
1,424 Views
PatrickLai
Contributor III
need to reinstall the driver for the device
0 Kudos
Reply