LPC55S28 - cannot connect debugger or enter ISP mode after disabling secure boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S28 - cannot connect debugger or enter ISP mode after disabling secure boot

3,038件の閲覧回数
awseiger
Contributor I

Hello,

I have been trying to get to the bottom of my inability to attach to a running LPC55S28 target and issue a device reset, and I tried disabling secure boot in the CFPA.

I did this and power-cycled my board, and now the MCU will not enter ISP mode, or allow my J-Link to connect. When issuing "connect" on my J-link I get the following error:

awseiger_0-1628796704290.png

 

I tried running some of the debug mailbox commands outlined in the user manual, but I could not get these to complete successfully.

Thanks,

Alex

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,012件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Same case with salesforce.

0 件の賞賛
返信

3,034件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello awseiger,

If chip can't enter ISP mode, maybe chip is broken, or disabled ISP mode:

Alice_Yang_0-1628839774542.png

 

BR

Alice

 

0 件の賞賛
返信

3,030件の閲覧回数
awseiger
Contributor I

Alice,

Prior to power cycling the MCU, I did a full read-back of the CMPA. Word 0 in the CMPA was all zeros, so ISP mode was absolutely enabled.

Alex

0 件の賞賛
返信