LPC55S28 Oscillator Requirements with High Speed USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S28 Oscillator Requirements with High Speed USB

Jump to solution
1,939 Views
zach890
Contributor I

I'm working on a new design with the LPC55S28 that will be utilizing high speed USB for data connections. Reading the data sheet and the user guide it's not completely clear what the external oscillator requirements are for the chip.

Both the data sheet and the user guide refer to the high speed USB clock as the 16MHz clock but section 45 (USB Phy) of the user guide mentions that XO32M can be configured to 16, 19.2, 20, 24, or 32MHz. Does this mean that an external crystal oscillator can operate at any of those frequencies or does it have to be 16MHz? Alternatively is an external oscillator needed for high speed USB the datasheet and user guide implies that it is a requirement.

Thanks for the help!

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
1,926 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

"Does this mean that an external crystal oscillator can operate at any of those frequencies"

->> Yes.

 

 

View solution in original post

0 Kudos
Reply
1 Reply
1,927 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

"Does this mean that an external crystal oscillator can operate at any of those frequencies"

->> Yes.

 

 

0 Kudos
Reply