LPC55S28-EVK USB0 ISP mode not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S28-EVK USB0 ISP mode not working

1,971件の閲覧回数
philippe_michon
Contributor I

Hello

I'm experimenting with the LPCxpresso55S28-EVK and was now testing the ISP functionality. I've now noticed that the USB ISP mode only works when using USB1 and not on USB0.

Pressing button ISP while plugin in P10 (USB0) doesn't have any response on my PC.

Pressing button ISP while plugin in P9 (USB1 both FS and HS) does work, the drivers are loaded and the device is available.

On my design I use only the USB0 and not USB1 , and the ISP mode is necessary for us 

component présent on the evaluation Bord  => lpc55S28jdb100 rev  is SD19271B.

component présent on my bord   => lpc5526jev98 BGA rev  is SD20381B

How activate the USB0 in ISP mode ?

There is an existing topic with a similare problem "LPC55S69-EVK USB0 ISP mode not working" is the same problem ?

regards

ラベル(1)
0 件の賞賛
返信
1 返信

1,963件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

We don't recommend use USB0 ISP mode, about detail please have a look at:

 

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC55-Don-t-Use-ISP-USB0-for-firmware-up... 

 

BR

Alice

0 件の賞賛
返信