LPC55S28-EVK USB Peripherals configurator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S28-EVK USB Peripherals configurator

Jump to solution
2,621 Views
_Ferrari_
Contributor V

Dear all,

I have a LPC55S28-EVK evaluation board and I would like to configure the pins 99,98,97 and 96 as USB VCOM device.

Starting from led_blinky simple project and using the peripherals configurator included in MCUXpresso IDE v11.5.1_7266 (Windows version) I tryed to add USB VCOM feature to the board without success.

I'm new in NPX platform so I think that some mistake was occurred during the pheripherals configuration.

So some questions:

1) Is it possible to use pins 99,98,97 and 96 as USB VCOM device ?

2) Do you have any simple NXP example thet shows how to use USB VCOM device peripherals configurator ?

Thank you very much for your help and cooperation

best regards

Luigi Ferrari

0 Kudos
Reply
1 Solution
2,595 Views
_Ferrari_
Contributor V

Dear all,

I downloaded the document "Using ConfigTool to create USB Project From Start.pdf" from this site and I fixed the problem. Using it I configured the USB0 port as VCOM device. Thank you very much for your help and cooperation, regards.

View solution in original post

0 Kudos
Reply
3 Replies
2,596 Views
_Ferrari_
Contributor V

Dear all,

I downloaded the document "Using ConfigTool to create USB Project From Start.pdf" from this site and I fixed the problem. Using it I configured the USB0 port as VCOM device. Thank you very much for your help and cooperation, regards.

0 Kudos
Reply
2,615 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi @_Ferrari_ ,

Could you please try the VCOM examples available in the SDK? These examples might help you with your application.

DanielRuvalcaba_0-1656352930382.png

Please take a look to the Config Tools quick reference guide to understand how to configure pins, clocks and peripherals in MCUXpresso.

Best regards, Daniel.

0 Kudos
Reply
2,613 Views
_Ferrari_
Contributor V

Dear all, I already tried the VCOM examples available in the SDK that work. Unfortunately it seems that they are not developed using peripherals configurator.

I'm working on new project that will use LPC55S26JBD64 processor but the hardware platform is not ready. So my idea is to fine tune the periferals driver on LPC55S28-EVK using the peripherals configurator and then apply the same procesure in the final target. (of course if it is possible).

Thank you very much for your help and cooperation.
best regards,

0 Kudos
Reply