LPC55S28 DMA0 How to modify the transmission format

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S28 DMA0 How to modify the transmission format

1,941 Views
MHY_0878
Contributor I

Hello NXP developers, I am an NXP, I am using LPC55S28 to implement DMA to transmit I2S data, I found that the I2S of NXP's official SDK uses DMA to transmit 16 bits, I don't know how to modify it to 24 bits, please guide us. Thank you (bow). A portion of the code is also attached.

//Configuration of I2S
I2S_TxGetDefaultConfig(&s_TxConfig);
                s_TxConfig.divider     = DEMO_I2S_CLOCK_DIVIDER;
                s_TxConfig.masterSlave = DEMO_I2S_TX_MODE;
                s_TxConfig.dataLength  = DataLenth;
                s_TxConfig.frameLength = FrameLength;
                s_TxConfig.leftJust    = false;
                I2S_TxInit(DEMO_I2S_TX, &s_TxConfig);

                I2S_RxGetDefaultConfig(&s_RxConfig);
                s_RxConfig.divider     = DEMO_I2S_CLOCK_DIVIDER;
                s_RxConfig.masterSlave = DEMO_I2S_RX_MODE;
                s_RxConfig.dataLength  = DataLenth;
                s_RxConfig.frameLength = FrameLength;
                s_RxConfig.leftJust    = false;
                I2S_RxInit(DEMO_I2S_RX, &s_RxConfig);

                PRINTF("AUDIO Loopback started!\r\n");
                PRINTF("Headphones will play what is input into Audio Line-In connector.\r\n");
//                        PRINTF("CLOCK_GetPll0OutFreq = %d\r\n", CLOCK_GetPll0OutFreq);

                s_RxTransfer.data     = &s_Buffer[0];
                s_RxTransfer.dataSize = sizeof(s_Buffer);
//                        s_TxTransfer.data     = &s_Buffer[0];
//                        s_TxTransfer.dataSize = sizeof(s_Buffer);

#if I2S_24BIT
//  24bit
                s_TxTransfer.data     = &sin_24bit[0];
                s_TxTransfer.dataSize = sizeof(sin_24bit);
#else
//  16bit
                s_TxTransfer.data     = &sin_16bit[0];
                s_TxTransfer.dataSize = sizeof(sin_16bit);
#endif


//Configuration of DMA0
#if DMA_Transfer

                DMA_Init(DEMO_DMA);

                DMA_EnableChannel(DEMO_DMA, DEMO_I2S_TX_CHANNEL);
                DMA_EnableChannel(DEMO_DMA, DEMO_I2S_RX_CHANNEL);
               
                DMA_SetChannelPriority(DEMO_DMA, DEMO_I2S_TX_CHANNEL, kDMA_ChannelPriority2);
                DMA_SetChannelPriority(DEMO_DMA, DEMO_I2S_RX_CHANNEL, kDMA_ChannelPriority3);
               
                DMA_CreateHandle(&s_DmaTxHandle, DEMO_DMA, DEMO_I2S_TX_CHANNEL);
                DMA_CreateHandle(&s_DmaRxHandle, DEMO_DMA, DEMO_I2S_RX_CHANNEL);
               
                I2S_TxTransferCreateHandleDMA(DEMO_I2S_TX, &s_TxHandle, &s_DmaTxHandle, TxCallback, (void *)&s_TxTransfer);
                I2S_TxTransferCreateHandleDMA(DEMO_I2S_RX, &s_RxHandle, &s_DmaRxHandle, RxCallback, (void *)&s_RxTransfer);
       
                /* need to queue two transmit buffers so when the first one
                 * finishes transfer, the other immediatelly starts */
                I2S_TxTransferSendDMA(DEMO_I2S_TX, &s_TxHandle, s_TxTransfer);
                I2S_TxTransferSendDMA(DEMO_I2S_TX, &s_TxHandle, s_TxTransfer);
       
          //I2S_TxTransferSendDMA(DEMO_I2S_TX, &s_TxHandle, s_TxTransfer);
                I2S_RxTransferReceiveDMA(DEMO_I2S_RX, &s_RxHandle, s_RxTransfer);
                I2S_RxTransferReceiveDMA(DEMO_I2S_RX, &s_RxHandle, s_RxTransfer);

#else   //I2STransfer
                I2S_TxTransferCreateHandle(DEMO_I2S_TX, &s_TxHandle, TxCallback, (void *)&s_TxTransfer);
                I2S_RxTransferCreateHandle(DEMO_I2S_RX, &s_RxHandle, RxCallback, (void *)&s_RxTransfer);

                I2S_RxTransferNonBlocking(DEMO_I2S_RX, &s_RxHandle, s_RxTransfer);
                I2S_TxTransferNonBlocking(DEMO_I2S_TX, &s_TxHandle, s_TxTransfer);
#endif       


//Also attach my project code

 

0 Kudos
Reply
4 Replies

1,907 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @MHY_0878 

About the I2S Configuration Adjustments.

#define DataLenth    24  // 24 bits per channel
#define FrameLength  64  // 64 bits per frame (32 bits per channel)

About the DMA Configuration,

You need to configure DMA for ​32-bit transfers​ since each sample is stored in a 32-bit word. 

Snipaste_2025-03-05_17-26-13.pngSnipaste_2025-03-05_17-26-13.png

You need to check this function.

BR

Harry

 

0 Kudos
Reply

1,901 Views
MHY_0878
Contributor I

Hello, I've seen this function, I found that it seems that only the modified I2S is used, I generate 16-bit and 24-bit positive sine waves in MCU lpc55S28 for testing, the 16-bit positive sine wave data is normal to transmit with I2S and DMA, but the 24-bit positive sine wave data is transmitted, only the I2S transmission waveform is correct, and the DMA transmission waveform is abnormal, I don't know what the reason is, please help me.

0 Kudos
Reply

1,903 Views
MHY_0878
Contributor I
Hello, I've seen this function, I found that it seems that only the modified I2S is used, I generate 16-bit and 24-bit positive sine waves in MCU lpc55S28 for testing, the 16-bit positive sine wave data is normal to transmit with I2S and DMA, but the 24-bit positive sine wave data is transmitted, only the I2S transmission waveform is correct, and the DMA transmission waveform is abnormal, I don't know what the reason is, please help me.
0 Kudos
Reply

1,865 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @MHY_0878 

I checked the i2s DMA code, 

bytesPerFrame is determined based on the width of i2s, so there is no need to modify it.

"the DMA transmission waveform is abnormal"

How do you test DMA waveforms? Can you send photos of the relevant waveforms?

BR

Harry

0 Kudos
Reply