LPC55S1x crystal less USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S1x crystal less USB

ソリューションへジャンプ
3,525件の閲覧回数
janpieterderuit
Contributor IV

Hi,

I'm going to try to implement the LPC55S1x crystal less Fullspeed USB, according to TN00065.

However, I can't find anything related to crystalless USB in the mentioned example (usb_device_composite_hid_audio_unified).
Also from the technical note it's not fully clear how to implement this feature. (i.e. should I replace libpower_softabi with libfro_calib_softabi.a, or should I use both?).

Does anyone know where I can find a working example?

Thanks in advance.

Best regards,
Jan Pieter de Ruiter
Airios

0 件の賞賛
返信
1 解決策
3,512件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I agree with you, I have checked the project: lpcxpresso55s16_dev_composite_hid_audio_unified_freertos, the project just uses the 96MHz fro_hf internal clock as the USB0 device clock(which is divided by 2 so that the USB0_CLK is 48MHz). The USB device frame signal is NOT used to adjust the 96MHz fro_hf in the project.

Regarding the high speed USB1, customer has to use external clock or crystal to provide high precious clock frequency, internal FRO clock can not be used.

Hope it can help you

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,522件の閲覧回数
janpieterderuit
Contributor IV

And can USB1 also be used without an external crystal (in Fullspeed mode)?
Or only USB0?
I guess USB1 can't run crystalless, since USB1_PHY needs a 16 - 32 MHz crystal oscillator, right?

0 件の賞賛
返信
3,513件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I agree with you, I have checked the project: lpcxpresso55s16_dev_composite_hid_audio_unified_freertos, the project just uses the 96MHz fro_hf internal clock as the USB0 device clock(which is divided by 2 so that the USB0_CLK is 48MHz). The USB device frame signal is NOT used to adjust the 96MHz fro_hf in the project.

Regarding the high speed USB1, customer has to use external clock or crystal to provide high precious clock frequency, internal FRO clock can not be used.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信
3,506件の閲覧回数
janpieterderuit
Contributor IV

Hi XiangJun Rong,

Thanks for the quick reply.

So I'll try to figure it out myself. It doesn't look too complicated. I'll get back when I have it working.

Too bad it doesn't work with USB1, since that's the one we use on our PCB... Would have been nice when it was mentioned in the technical note (explicitly).

BR, Jan Pieter

0 件の賞賛
返信
3,483件の閲覧回数
janpieterderuit
Contributor IV

We decided to not implement crystalless USB for now, as USB0 is not available on our PCB, and routing restrictions will probably prevent changing that, even when we do a PCB redesign.

So I will not come back with an update about implementing it.

0 件の賞賛
返信