LPC55S16 MCAN Transmission Error Counter(TEC) registor Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S16 MCAN Transmission Error Counter(TEC) registor Issue

1,286 Views
jmorel
Contributor II

Im facing an issue were my transmissions are having the data field cut out and the TEC register counts up to the 255 limit disabling the mcan Module. we've also ran into the issue with the Transmitter Delay Compensator Registor(TDCR) where any value other than 0 would not allow the module to transmit anything.

jmorel_0-1719846510207.pngjmorel_0-1719846510207.png

.BaudRate = 1000000,
.BaudRateFD = 4000000,
.CanfdNormal = true,
/* CAN timing configuration */
.NominalScaler = 5,
.Segment1 = 19,
.Segment2 = 6,
.RSyncJumpwidth = 6,
/* CANFD timing configuration */
.DataScaler = 7,
.DataSegment1 = 2,
.DataSegment2 = 0,
.DataRSyncJumpwidth = 0,

Labels (2)
0 Kudos
Reply
1 Reply

1,249 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @jmorel 

For better help you check the issue, could you please send a project that can reproduce your issue on LPCXpresso55s16 board. 

 

BR

Alice

0 Kudos
Reply