LPC55S16-EVK CLI options

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S16-EVK CLI options

ソリューションへジャンプ
3,569件の閲覧回数
embedded_eng_
Contributor III

Hi,

I have a LPC55S16-EVK, and I'm using MCUXpresso IDE.

I'm trying to clean & build & flash the board (DFU-MODE) directly from my terminal (Ubuntu).

So far, I tried:

* clean the project with  "make -r clean -C Debug/"

This seems to work, I need to run "mcuxpressoide-11.3.0_5222/MCUXpressoPath.sh" script before the clean.

* build the project with "make -r -C Debug/ all"

Same as the clean, works and I need to run the path script before.

 

Now, in order to flash the board I've tried to use dfu-util.

dfu-util -d VVVV:PPPP -c 0 -t 2048 -R -D ??

VVVV - Vendor ID

PPPP - Product ID

I'm not sure which file I should pass to the command (instead of ??)

* I tried the axf file in Debug directory and the new program was not flashed to the MCU.

* I tried mcuxpressoide-11.3.0_5222/ide/plugins/com.nxp.mcuxpresso.tools.bin.linux_11.3.0.202101111545/binaries/LPC432x_CMSIS_DAP_V5_361.bin.hdr, and the old program was flashed into the MCU (the last one built directly from the IDE).

 

What am I missing here?

How should I flash the MCU in DFU mode?

My method to clean & build the project are correct? this should be made from the makefile in Debug directory?

 

P.S I tried the lpcscrypt-2.1.2_57/scripts/dfu_boot script and had the same issues.

タグ(3)
0 件の賞賛
返信
1 解決策
3,546件の閲覧回数
converse
Senior Contributor V

How about RTM? https://www.mouser.com/pdfDocs/UM11295.pdf

It states

On-chip ROM bootloader supports:
– Booting of images from on-chip flash.
– Supports CRC32 image integrity checking.
– Supports flash programming through In System Programming (ISP) commands over the following interfaces: USB0/1 interfaces using HID class device, UART interface (Flexcomm 0) with auto baud, SPI slave interfaces (Flexcomm 3 or 9) using mode 3 (CPOL = 1 and CPHA = 1), and I2C slave interface (Flexcomm 1).
– ROM API functions: Flash programming API, Power control API, and Secure firmware update API using the NXP Secure Boot file format, version 2.0 (SB2 files).
– Supports booting of images from PRINCE encrypted flash regions.
– Supports NXP Debug Authentication Protocol version 1.0 (RSA-2048) and 1.1
(RSA-4096).
– Supports setting a sealed part to Fault Analysis mode through Debug authentication.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,559件の閲覧回数
converse
Senior Contributor V

You can’t use dfu-util to program flash - only load code into RAM (which is typically a boot loader which could then be used to program flash). If you want to use command line only (why?) the read the MCUXpresso user manual chapter on command line flash programmer. You will need a debug probe, such as mculink or lpclink2.

0 件の賞賛
返信
3,550件の閲覧回数
embedded_eng_
Contributor III

Thanks for the reply.

So what are the MCU's boot modes/options?

Can it boot from USB?

I'm looking for a MCU to use in my PCB.

I need a option to upgrade the MCU's firmware without an external programmer.

 

0 件の賞賛
返信
3,547件の閲覧回数
converse
Senior Contributor V

How about RTM? https://www.mouser.com/pdfDocs/UM11295.pdf

It states

On-chip ROM bootloader supports:
– Booting of images from on-chip flash.
– Supports CRC32 image integrity checking.
– Supports flash programming through In System Programming (ISP) commands over the following interfaces: USB0/1 interfaces using HID class device, UART interface (Flexcomm 0) with auto baud, SPI slave interfaces (Flexcomm 3 or 9) using mode 3 (CPOL = 1 and CPHA = 1), and I2C slave interface (Flexcomm 1).
– ROM API functions: Flash programming API, Power control API, and Secure firmware update API using the NXP Secure Boot file format, version 2.0 (SB2 files).
– Supports booting of images from PRINCE encrypted flash regions.
– Supports NXP Debug Authentication Protocol version 1.0 (RSA-2048) and 1.1
(RSA-4096).
– Supports setting a sealed part to Fault Analysis mode through Debug authentication.

0 件の賞賛
返信
3,533件の閲覧回数
embedded_eng_
Contributor III

Thanks!

0 件の賞賛
返信