LPC55S16 - CCID?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S16 - CCID?

5,064 Views
ND2
Contributor III

Hello,

We are trying to get the LPC55S16 connected to a macOS over CCID interface.

The CCID interface firmware we have is working on Windows and Linux. Can you please support us on how we can resolve this issue?

Labels (1)
0 Kudos
Reply
4 Replies

4,993 Views
ND2
Contributor III

Hi @xiangjun_rong We already have a working code for the LPC55S16 that works fine on Linux and on Windows. That code doesn't work on the macOS. We need support to get the LPC55S16 communicating with the macOS (Apple processors and Intel Processors)

0 Kudos
Reply

4,988 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The Example code for CCID was developed by an AE engineer instead of SDK software team, because of resource and environment limited, the example code has not been tested on Mac os.

BR

XiangJun Rong

0 Kudos
Reply

5,001 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

This is CCID example developed by SE team based on LPC55S69, pls try to port it to LPC55S16 yourself.

I attach the example code here.

BR

XiangJun Rong

 

0 Kudos
Reply

4,960 Views
ND2
Contributor III

Hello @xiangjun_rong 

There doesn't seem to be a project file in it. Tried on Windows and macOS both.

See attached images

Let me know if I am missing something.

0 Kudos
Reply