LPC55S06 8 UART + 1 HS SPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S06 8 UART + 1 HS SPI

2,181件の閲覧回数
stefanardo
Contributor I

Hi,

I am trying to configure the LPC55S05JBD64 with 8 UART + 1 HS SPI but it seems it is impossible due to pin mux limitation? Is it true or I am making a mistake? 

If I try to configure FLEXCOMM 2 as UART  it seems RXD  can be routed only on P0_26 the same as HS_SPI_MOSI.

Do you have any suggestion?

 

Regards.

Stefano

 

0 件の賞賛
返信
3 返答(返信)

2,154件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I reviewed the information and am sorry, but this seems not possible.

Best regards,
Pavel

2,147件の閲覧回数
stefanardo
Contributor I

Thanks anyway Pavel, but I suggest to correct the information on the datasheet "UART up to 8, I2C up to 8, I2S up to 8 and SPI up to 6) + 1 HS SPI"  for my knowledge of english language means that the HS SPI is excluded from the count of usable flexcomm.

 

Regards.

0 件の賞賛
返信

2,168件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, let me get into your case and when I have more information, I will contact you.

Best regards,
Pavel

0 件の賞賛
返信