LPC553x Current Consumption Below 12 MHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC553x Current Consumption Below 12 MHz

1,182件の閲覧回数
mikenn
Contributor III

What's up NXP,

I am interested in LPC553x in a battery powered application.  Power consumption and battery longevity are paramount, and as such, I have a question about current consumption in active mode.  The data sheet specifies typical consumptions around 1-2mA at 12 MHz active mode but nothing is specified at lower frequencies.  This suggests there is no proportional reduction in current consumption as clock frequency tends towards zero.  ST completely characterizes their M33 parts at near zero clock speeds with ~100uA currents in active mode.  Can we have LPC553x current consumption at lower clock speeds please?

0 件の賞賛
返信
1 返信

1,169件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

When customers chooses LPC553x, as I most most user application system clock is higher than 12M, so we don't have the same statistic for CCLK lower than 12M. In this case, the current consumption must be lower than the consumption at 12M. 

I can escalate it as document improvement request to document team, but for the moment we don't have it. user needs to measure by self.

Thanks,

Jennie

0 件の賞賛
返信