LPC5536 SDK 2.15.100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
864件の閲覧回数
Bela1
Contributor III

Ladies and Gentlemen,

I'd like to inform You, that something is wrong with the SDK for LPC5536. Version 2.15.100 (today the newest) doesn't compile, when I create a whole new C project in MCUXpresso.

I saw some error message during project creation, but I didn't make a screenshot. After the project succesfully created, there's a "virgin" source code which doesn't compile. Some includes are missing: stdio.h, pin_mux.h, LPC5536.h.

Excuse me, I'm focusing on my own project, I couldn't make a deeper study to this failure. I tried to construct a new project more times, and I saw always the same symptom.

With 2.14, it is OK, everything works properly.

ラベル(1)
0 件の賞賛
返信
1 解決策
835件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Bela1 

Thanks for your reporting.

I created a new project based on MCUXpressso IDE v11.9.0, SDK2.15. Not find the issue after compile.

I attached the steps.

 

 

BR

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
836件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Bela1 

Thanks for your reporting.

I created a new project based on MCUXpressso IDE v11.9.0, SDK2.15. Not find the issue after compile.

I attached the steps.

 

 

BR

Alice

0 件の賞賛
返信