LPC5536 SCTIMER/PWM issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5536 SCTIMER/PWM issues

ソリューションへジャンプ
2,720件の閲覧回数
CatFather
Contributor I

SCTIMER.PNG

 I am controlling a bldc motor with 3 sct ouptuts. This works fine until one of the thrree duty cycles reach 50-60%. After this point strange things happen and it might be that pulses get missing (see attached red curve) The SCTIMER_UpdatePwmDutycycle function is called every 50us. (PWM Frequency is 20kHz). If I increase the frequency to 50kHz it gets even worse. If I choose frequency 10kHz it gets better but this frequency is not suitable for my application.

 

This is how I initialize the SCTIMER: 

   sctimer_config_t sctimerInfo;
   sctimer_pwm_signal_param_t pwmParam;
   uint32_t sctimerClock;
   
   s_PWMcallback = NoOp;
   
   sctimerClock = CLOCK_GetFreq(kCLOCK_BusClk);
   
   SCTIMER_GetDefaultConfig(&sctimerInfo);
   sctimerInfo.enableBidirection_l = TRUE;
   SCTIMER_Init(SCT0, &sctimerInfo);

   // Configure PWM params with frequency 20kHZ from output
   pwmParam.output           = PWM_OUT_A;
   pwmParam.level            = kSCTIMER_HighTrue;
   pwmParam.dutyCyclePercent = 0;
   if (SCTIMER_SetupPwm(SCT0, &pwmParam, kSCTIMER_CenterAlignedPwm, PWM_FREQ_HZ, sctimerClock, &s_eventNumberOutputA) == kStatus_Fail)
   {
      SetDeviceStatusWithErrorNumber(ERR_BIT_INIZIALISATION, 2);
      return ;
   }

   pwmParam.output           = PWM_OUT_B;
   pwmParam.level            = kSCTIMER_HighTrue;
   pwmParam.dutyCyclePercent = 0;
   if (SCTIMER_SetupPwm(SCT0, &pwmParam, kSCTIMER_CenterAlignedPwm, PWM_FREQ_HZ, sctimerClock, &s_eventNumberOutputB) == kStatus_Fail)
   {
      SetDeviceStatusWithErrorNumber(ERR_BIT_INIZIALISATION, 3);
      return ;
   }
   
   pwmParam.output           = PWM_OUT_C;
   pwmParam.level            = kSCTIMER_HighTrue;
   pwmParam.dutyCyclePercent = 0;
   if (SCTIMER_SetupPwm(SCT0, &pwmParam, kSCTIMER_CenterAlignedPwm, PWM_FREQ_HZ, sctimerClock, &s_eventNumberOutputC) == kStatus_Fail)
   {
      SetDeviceStatusWithErrorNumber(ERR_BIT_INIZIALISATION, 4);
      return ;
   }

   // Enable interrupt flag for event associated with out 4, we use the interrupt to update dutycycle
   EnableInterruptPWM();

   // Receive notification when event is triggered
   SCTIMER_SetCallback(SCT0, SCTIMER_HANDLER, s_eventNumberOutputA);
   
   
   NVIC_SetPriority(SCT0_IRQn, IRQPRIO_MOTOR_PWM); // prio[0..7] 0 is highest   // Enable at the NVIC
   EnableIRQ(SCT0_IRQn);
   
   // Start the 32-bit unify timer
   SCTIMER_StartTimer(SCT0, kSCTIMER_Counter_U);    
 
 
And this is how I Update the pulse width(called from interrupt):
 
   DisableInterruptPWM();
   SCTIMER_UpdatePwmDutycycle(SCT0, PWM_OUT_A, (UInt8)(pwmA*100), s_eventNumberOutputA);
   SCTIMER_UpdatePwmDutycycle(SCT0, PWM_OUT_B, (UInt8)(pwmB*100), s_eventNumberOutputB);
   SCTIMER_UpdatePwmDutycycle(SCT0, PWM_OUT_C, (UInt8)(pwmC*100), s_eventNumberOutputC);
   EnableInterruptPWM();
 
For any ideas I am very thankful.
 
Rico
ラベル(1)
0 件の賞賛
返信
1 解決策
2,684件の閲覧回数
CatFather
Contributor I

I managed to resolve this issue by commenting the update of MATCH register and just update the MATCHREL register

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,685件の閲覧回数
CatFather
Contributor I

I managed to resolve this issue by commenting the update of MATCH register and just update the MATCHREL register

0 件の賞賛
返信