LPC5536 DMA transfers less data than expeced

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5536 DMA transfers less data than expeced

4,375件の閲覧回数
orange_chris
Contributor II

Hello,

I have an application with the LPC5536 where I have to sample 3 ADC channels in rapid succession at 3 very distinct points of time. The idea is to trigger them with a SCT channel, collect the 9 (3 x 3) values in the FIFO of the ADC and transfer them off to memory using the DMA when the conversion has finished. However I have run into a problem I don't understand.

I have removed the triggering of the ADC via the SCT for now for easier debugging control. I have set up 3 ADC channels as a sequence with the FIFO watermark set to 8 so that the DMA request happens after the 9th byte

lpadc_conv_command_config_t ADCCommand1 = {kLPADC_SampleChannelSingleEndSideA, 1U, 2, false, 0UL, kLPADC_HardwareAverageCount1, kLPADC_SampleTimeADCK3, kLPADC_HardwareCompareDisabled, 0UL, 0UL, kLPADC_ConversionResolutionStandard, false};

lpadc_conv_command_config_t ADCCommand2 = {kLPADC_SampleChannelSingleEndSideA, 3U, 3, false, 0UL, kLPADC_HardwareAverageCount1, kLPADC_SampleTimeADCK3, kLPADC_HardwareCompareDisabled, 0UL, 0UL, kLPADC_ConversionResolutionStandard, false};

lpadc_conv_command_config_t ADCCommand3  = {kLPADC_SampleChannelSingleEndSideA, 8U, 0, false, 0UL, kLPADC_HardwareAverageCount1, kLPADC_SampleTimeADCK3, kLPADC_HardwareCompareDisabled, 0UL, 0UL, kLPADC_ConversionResolutionStandard, false};

LPADC_SetConvCommandConfig(ADC0, 1, &ADCCommand1);
LPADC_SetConvCommandConfig(ADC0, 2, &ADCCommand2);
LPADC_SetConvCommandConfig(ADC0, 3, &ADCCommand3);

const lpadc_config_t ADC_Config = {true, kLPADC_ConversionAverage1, true, 0x80UL, kLPADC_ReferenceVoltageAlt3, kLPADC_PowerLevelAlt1, kLPADC_TriggerPriorityPreemptImmediately, false, 0UL, 8UL, 0UL};
LPADC_Init(ADC0, &ADC_Config);

LPADC_EnableFIFO0WatermarkDMA(ADC0, true);

I have also set up a DMA channel to transfer the data:

g_XferConfig = DMA_CHANNEL_XFER(false, true, false, false, sizeof(uint32_t), kDMA_AddressInterleave0xWidth, kDMA_AddressInterleave1xWidth, 9 * sizeof(uint32_t));

DMA_PrepareChannelTransfer(&DMAChannelConfigStruct, (void*)(&(BSP_SENSOR_ADC->RESFIFO[0])), (void *)Sensor_ADC_Buffer, g_XferConfig, kDMA_PeripheralToMemory, NULL, NULL);
(void)DMA_SubmitChannelTransfer(&ADC_DMA_Handle, &DMAChannelConfigStruct);

  • The behaviour if I trigger the ADC via software trigger is:
    I can see the ADC sampling 3 values on each trigger as expected (by watching the FIFO level register)
  • On the first 2 triggers no data is transfered as expected since the FIFO level is still below the threshold
  • On the 3rd trigger data is transfered via the DMA but only 3 uint32_t values instead of the expected 9
  • As a consequnence, the FIFO level is only lowered by 3 and not down to zero as expected and a a consequence of that on every further trigger 3 more values are transfered and the FIFO level always bonces up and down but the FIFO never gets emptied.

Why does the DMA transfer only a third of the bytes configured? The "9 * sizeof(uint32_t)" bytes in the xfer config look correct to me and they are correctly converted into 9 transfers (leading to the XFERCOUNT field in the XFERCFG register set to 8).

Up front, I am not allowed to upload my project and it is on a custom hardware and not on an evaluation board anyway.

EDIT: I have noticed that I did not have the DMA_SetupDescriptor() call like in the lpadc_dma example and have added that but the behaviour did not change. I still wonder what the descriptors do because the SRAMBASE register mentioned in the RM always points to the s_dma_descriptor_table0 table in the library.

ラベル(1)
タグ(1)
6 返答(返信)

2,794件の閲覧回数
nobodyKnows
Contributor III

Hi,

I have the same issue. For one request I get 3 reads. Could you share the solution?

Thanks a lot.

4,324件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @orange_chris 

How many time reads RESFIFO for one DMA trigger?

The FIFO can be emptied by successive reads of RESFIFO.

 

BR

Alice

0 件の賞賛
返信

4,295件の閲覧回数
orange_chris
Contributor II

Hello Alice,

it seems that the RESFIFO is read 3 times per DMA trigger despite being configured to be read 9 times with

g_XferConfig = DMA_CHANNEL_XFER(false, true, true, false, sizeof(uint32_t), kDMA_AddressInterleave0xWidth, kDMA_AddressInterleave1xWidth, 9 * sizeof(uint32_t));

There is data left in the RESFIFO, I have checked that using manual reads after the DMA was triggered

I can scale the reads down to 1 and 2 replacing the 9 in the config above by 1 and 2 but starting at 4, the DMA only reads 3 times.

Is there a hidden limit on how many bytes can be transfered per DMA trigger?

4,264件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @orange_chris 

How about first change and tested base on adc_dma demo under SDK, if still can't work as your requirements, send the project to me , I help to check on LPCxpresso5536-evk board, I think it is easy to find problem by debugging.

 

BR

Alice

 

0 件の賞賛
返信

4,214件の閲覧回数
orange_chris
Contributor II

Hello Alice,

I have found out that it is trivial to reproduce. Just open the lpadc_demo project from the SDK and increase DEMO_CADC_SAMPLE_COUNT to anything above 3. You will see that the ADC indeed samples additional sample but they are never transfered into RAM despite the transfer being configured to be DEMO_CADC_SAMPLE_COUNT * sizeof(uint32_t) bytes.

BR,
Christian

3,995件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @orange_chris 

Sorry to reply you late, I came back from public holiday yesterday, and I know Guenter is helping you about this case, he will tell you the answer .ASAP.

 

BR

Alice

0 件の賞賛
返信