LPC5534 cannot write CMPA for CAN_BAUD_RATE config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5534 cannot write CMPA for CAN_BAUD_RATE config

1,175 Views
briandavidson1
Contributor II

Hello!

We are currently struggling to write CMPA to fix the CAN_BAUD for the bootloader. Accessing through ISP and "get-property", "flash-image" and "flash-erase-all" work fine, but when trying to perform a "write-memory" on the CMPA region it fails with invalid_argument:

>>blhost -p COM3 get-property 1
Ping responded in 1 attempt(s)
Inject command 'get-property'
Response status = 0 (0x0) Success.
Response word 1 = 1258488064 (0x4b030100)
Current Version = K3.1.0

>>blhost -p COM3 write-memory 0x3E204 {{00}}
Ping responded in 1 attempt(s)
Inject command 'write-memory'
Successful generic response to command 'write-memory'
(1/1)100% Completed!
Response status = 4 (0x4) kStatus_InvalidArgument
Wrote 1 of 1 bytes.

>>blhost -p COM3 write-memory 0x3E204 {{00040000}}
Ping responded in 1 attempt(s)
Inject command 'write-memory'
Successful generic response to command 'write-memory'
(1/1)100% Completed!
Response status = 4 (0x4) kStatus_InvalidArgument
Wrote 4 of 4 bytes.

Trying to write anything will always read back "00"

 

Any hints why it won't work? Thanks in advance and kind regards!

0 Kudos
Reply
1 Reply

1,155 Views
briandavidson1
Contributor II

OK, I think I finally found a solution. It looks like the CMPA has to be written as a single block.

 blhost -p COM3 write-memory 0x3E200 cmpa.bin

Works even though only a single bit is changed. I think it should be mentioned somewhere that it is not possible to write bytes or words to CMPA. Ideally, blhost should automatically perform a read-modify-write operation in such cases...

0 Kudos
Reply