LPC552x/S2x: Pacing by DMA requests

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC552x/S2x: Pacing by DMA requests

3,369件の閲覧回数
dmaeda
Contributor I

Pacing by DMA requests for serial interfaces such as USART, I2C and I2S is described below by DMATX and DMARX in the FIFOCFG register.

For DMATX:
"Generate a DMA request for the transmit function if the FIFO is not full."

For DMARX:
"Generate a DMA request for the receive function if the FIFO is not empty."

On the other hand, each of TXLVL and RXLVL in the FIFOTRIG register can define each FIFO level trigger point.

I have tested using the USART DMA example in the SDK and it seems that a DMA request is generated for each data send/receive, regardless of TXLVL and RXLVL.

I understand that TXLVL and RXLVL are ignored for pacing by DMA requests and that burst transfer by DMA request is not supported, is that correct?

Best regards,

Daisuke

 

0 件の賞賛
返信
6 返答(返信)

3,350件の閲覧回数
dmaeda
Contributor I

I have contacted TIC support about this.

0 件の賞賛
返信

3,339件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, let me review your information, only for being sure could you tell me the example are you based on?

Best regards,
Pavel

0 件の賞賛
返信

3,307件の閲覧回数
dmaeda
Contributor I

Dear Pavel-san,

Thank you for your daily support.

I would appreciate it if you respond to my case in TIC instead of this case.

Best regards,

Daisuke

 

0 件の賞賛
返信

3,296件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

I saw you have 3 cases with some differences in the DMA, for quality of service I will be following your case in one of these.

Best regards,
Pavel

0 件の賞賛
返信

3,291件の閲覧回数
dmaeda
Contributor I
Dear Pavel-san,

Thank you for your reply and daily support.

I would appreciate it if you respond to my cases in TIC.

Could you close this case?

Best regards,

Daisuke
0 件の賞賛
返信

3,323件の閲覧回数
dmaeda
Contributor I

Hi Pavel-san,

Thank you for your reply.

In the example below in the SDK, even if RXLVL is a value other than 0 (config.rxWatermark ≠ kUSART_RxFifo1), one data is always transferred to the destination buffer each time it is received (key input). RXLVL seems to be ignored by DMA.

\SDK_2_12_0_LPCXpresso55S28\boards\lpcxpresso55s28\driver_examples\usart\dma_double_buffer_transfer

/* Initialize the USART. */
/*
* config.baudRate_Bps = 115200U;
* config.parityMode = kUSART_ParityDisabled;
* config.stopBitCount = kUSART_OneStopBit;
* config.txFifoWatermark = 0;
* config.rxFifoWatermark = 1;
* config.enableTx = false;
* config.enableRx = false;
*/
USART_GetDefaultConfig(&config);
config.baudRate_Bps = BOARD_DEBUG_UART_BAUDRATE;
config.enableTx = true;
config.enableRx = true;
config.rxWatermark = kUSART_RxFifo8;

USART_Init(DEMO_USART, &config, DEMO_USART_CLK_FREQ);
USART_EnableRxDMA(DEMO_USART, true);

Best Regards,

Daisuke

 

0 件の賞賛
返信