LPC5528 USB1 as full speed device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC5528 USB1 as full speed device

跳至解决方案
1,439 次查看
tks11111
Contributor II

Hi All, 

I found a thread that discussed how to use USB1 as a full-speed device.

LPC55S6x USB1 as full speed device - NXP Community

Do I need to change the clock setting if I set the bit 21 of the USB1 device command/status register (DEVCMDSTAT) to 1?
Also, do I need to add any other speed configuration?

Appreciate any help.

Thanks.

 

BR,

Peter 

标签 (2)
0 项奖励
回复
1 解答
1,383 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI tks11111,

There is no need setting clock. 

To set LPC5528 USB1 as full speed device, setting Forced FS bit as 1 is enough.

Best Regards,

Jun Zhang

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,384 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI tks11111,

There is no need setting clock. 

To set LPC5528 USB1 as full speed device, setting Forced FS bit as 1 is enough.

Best Regards,

Jun Zhang

0 项奖励
回复